cancel
Showing results for 
Search instead for 
Did you mean: 

MEMS Studio reports WHO_AM_I issue when using LSM6DSO16IS Sensor Hub

Torris-Yin
Associate II

I am using NUCLEO_F401RE + X-NUCLEO-IKS4A1 with MEMS Studio software. 

X-NUCLEO-IKS4A1 offers multiple various bus configurations, including the sensor hub mode for LSM6DSO16IS.

TorrisYin_0-1729055728000.png

TorrisYin_1-1729055739422.png

However, only in standard I2C mode can we establish the connection in MEMS Studio. If using the sensor hub mode, there will be WHO_AM_I warning and connection cannot be setup.

The issue doesn't appear in Unicleo-GUI since we can disable the sensor affected, but in MEMS Studio, the option cannot be changed.

TorrisYin_2-1729056098005.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Torris-Yin ,

Unfortunately, it is not possible to do this in MEMS Studio, which is why the sensor is not recognized.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Torris-Yin
Associate II

WHO_AM_I Warning:

TorrisYin_0-1729056334010.png

 

Hi @Torris-Yin ,

Unfortunately, it is not possible to do this in MEMS Studio, which is why the sensor is not recognized.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.