2013-08-21 3:23 PM
I'm using a LPS331 in a prototype. The datasheet does not give any timing information other than one can select the output data rate. What are the timing values for SPI such as max clocking frequency, etc. I search ST site and could not find any other information that would help. For I2C it says it complies with fast mode (400kHz) but nothing for SPI.
Thanks, Tom #mems-barometer2013-08-23 7:42 AM
Please note that this forum is specifically for MEMS Microphones and not for generic MEMS sensors. Anyhow, the LPS331AP max SPI clock frequency is 10MHz.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.