2017-05-07 4:17 PM
The LSM9DS1 data sheet shows that the accelerometer/gyroscope module's two interrupts can be configured either as open-drain or push/pull. However, I am missing the description of the magnetometer module's interrupt. I assume that means it is fixed and cannot be user-configured. Is it fixed as open-drain type, or as push/pull type?
#interrupts #lsm9ds1 #push-pull-output-or-open-drain-outputSolved! Go to Solution.
2017-05-19 9:06 AM
The INT_M interrupt pin is also push-pull.
2017-05-10 6:52 AM
The DRDY_M (Magnetic sensor data ready) pin is push-pull, with active high level.
2017-05-10 1:12 PM
Thanks, that helps. But I was actually asking about the magnetometer interrupt, Pin 10, INT_M. I couldn't find anything in the data sheet saying whether it's push-pull or open drain. The active level (high/low) can be configured in software but not, apparently, the output type. Do you know which it is?
2017-05-19 9:06 AM
The INT_M interrupt pin is also push-pull.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.