2016-04-06 6:52 AM
Hello,
new in this pressure are, for absolute pressure measurement. is the LPS25HB in free air will give 760hpar reading? for example, if I put it in a flat balloon, the reading will be 760hpar, if I start to blow the balloon, then the reading increase from 760hpar. is this the way absolute pressure works. Sincerely, David Sun #lps25hb2016-04-07 1:37 AM
Hello David,
yes, you will basically be able to read whatever pressure you have within the baloon. More in general, given that the LPS25H is in a closed environment on which you force a given pressure, you can reliably measure whatever value within the 200 to 1260hPa range. Regards, AdalbertoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.