2016-10-03 9:03 AM
Hi,
in datasheet for LPS25HB ('DocID027112 Rev 3'), page 27, the register 'RES_CONF (10h) Pressure and temperature resolution' is described. Question1: Is the 'Nr. internal average' (table 18) applicable for One-shot mode? Q2: If it is so, would be selected Nr.internal average influence on conversion time for One-shot mode at all? Q3: How long would be conversion time in One-shot mode? If there is concerned above influence (see Q2), what is the conversion time, when Nr.internal average=8 and when Nr.internal average=512? Best regards. #lps25hb #pressure-sensorWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.