2023-07-04 5:30 AM
Hello,
We want to operate the LPS22HB pressure sensor with the i2c protocol. The pin legs of the sensor are connected to the SCL - SDA 4.7k ohm pull-up resistors. Sa0/GND Csi / 3.3 RES / GND. This is how connections are made. This way we can't get data from the sensor. What is the reason of this?
2023-07-06 7:58 AM
Hi @Sinoplu57 ,
In alternative you can try to reduce the pull up resistances, for example you can use 2.2kOhm.
Let me know if this solves.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.