cancel
Showing results for 
Search instead for 
Did you mean: 

LPS22DF: Polarity of INT_DRDY pin?

tcachat
Associate II

I would like to change the state of the INT_DRDY of LPS22DF. I have tried to change the value of INT_H_L bit in register CTRL_REG3 (12h), but it has no (immediate) effect. Is it necessary to activate the pin? I have also tried different values in CTRL_REG4 (13h), without effect.

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
tcachat
Associate II

Sorry, I just found the INT_EN_I3C bit in IF_CTRL (0Eh).

View solution in original post

1 REPLY 1
tcachat
Associate II

Sorry, I just found the INT_EN_I3C bit in IF_CTRL (0Eh).

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.