2016-10-16 2:59 AM
The LIS3DSH has a three channel 10 bit A/D converter but I can't find any information on it.
What is the accuracy? (I could tie one channel to a voltage reference for calibration if necessary) What is the input voltage range? What is the maximum input current? (will I need to buffer the channels) #lis3dsh2016-10-17 2:59 AM
I suppose you mean LIS3DH, because LIS3DSH does not have auxiliary ADC.
Then you can check this: [DEAD LINK /public/STe2ecommunities/mems_sensors/Lists/Accelerometers/Flat.aspx?RootFolder=/public/STe2ecommunities/mems_sensors/Lists/Accelerometers/LIS3DH%20ADC%20Specifications&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580004224A862E061BB4BADDEF313D70857E6&TopicsView=https://my.st.com/public/STe2ecommunities/mems_sensors/Lists/Accelerometers/AllItems.aspx¤tviews=316]https://my.st.com/public/STe2ecommunities/mems_sensors/Lists/Accelerometers/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmems_sensors%2fLists%2fAccelerometers%2fLIS3DH%20ADC%20Specifications&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580004224A862E061BB4BADDEF313D70857E6&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmems_sensors%2FLists%2FAccelerometers%2FAllItems%2Easpx¤tviews=316
Best regards
Miroslav
2016-10-17 10:18 AM
Thanks 1,200mV, +-400mV, 8 or 10 bit depending on mode. The input current is not mentioned though so I will assume that it does need buffering. Thanks for correcting the part number.
2025-01-05 8:49 PM
Hi, Miroslav,
I have same question about the ADC's accuracy, but I couldn't open the link above.
Could you send me a updated link? or, if just let me know the ADC's accuracy. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.