2019-10-18 7:07 AM
Hi,
Is it possible to disable the interrupt line? By default it is Default: push-pull output forced to GND but I would like to be able to make it floating to use the ucontroller gpio connected to INT1 for other purposes like UART TX.
Thank you
2019-10-21 2:05 AM
Hi @josescxavier , do you mean change the INT1 internal config from push-pull to open-drain? Unfortunately is not possible... please note that even if the pull down to gnd is very weak, the use of INT1 pin routed to UART com could cause a little x-talk. Better to leave it unconnected, even if I suspect it would require a HW rework. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.