2022-05-10 1:33 AM
We have performed the self test on two prototype boards,
as instructed in this post: https://community.st.com/s/question/0D50X00009XkXegSAF/lis331hh-understanding-self-test
The x and y differences are around 135, which is in the range, but on the z axis we get around 380, which according to the datasheet, is just enough to no pass the self test.
The datasheet also specifies that the "Self-test output changes with the power supply" and that the product was calibrated at 2.5V.
Our question is the following:
Can the fact that we use a different supply voltage (3.3V) be the reason why the self test (just barely) fails or does the range of the self test already account for potencial differences?
Best regards!
2022-05-10 6:50 AM
Hi @Sašo Vozli�? ,
are both the prototype boards failing the self test?
And did you follow the self test procedure as suggested on the C drivers on Github --> lis331dlh_self_test.c?
The Vdd could slightly impact the data on this product, but should not make the difference between pass and fail. Please be sure to be in a controlled environment during the self test.
-Eleon
2022-05-11 5:22 AM
Hi Eleon,
yes, both are failing the self test. We'll try to run a test with 2.5V instead of 3.3V.
We did follow the procedure.
On a related note, how does a negative self test sign impact the results?
Do we just change the sign on the specified ranges?
Do we have to run the self test in both directions?
PS: If the self test fails with the positive sign, but passed with the negative one, how do we interpert that?
Best regards,
Sašo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.