2025-01-30 4:43 AM
HI, it seems to me that reading the LIS2MDL sensor only works correctly if I read first the X axis, then the Y axis, and finally the Z axis separately, each axis in a separate SPI transaction.
Solved! Go to Solution.
2025-01-31 3:40 AM
Problem solved
I found similar topic: https://community.st.com/t5/stm32-mcus-products/stm32f767-spi-bidirectional-receive-mode-more-spi-clocks-are/m-p/213384#M46791
And this description why STM32HAL cant handle bidirectional SPI properly:
http://efton.sk/STM32/gotcha/g32.html
2025-01-30 6:00 AM
Hi, I tried printing out raw values.
Below you can see 3 samples with broken Z axis readout, each time it was broken the MSB of Z axis was equal to LSB of X axis. This might be a problem with my software, but if you guys now know how LIS2MDL registers are upgraded and how BDU works you can make me sure that this is not LIS2MDL problem but my software problem... I would be grateful if you could take a look at these results and assess whether this is a LIS2MDL problem.
Magn X | Magn Y | Magn Z | Raw data X | Raw data Y | Raw data Z |
------------------------------------------------------------------
-975, | 171, | 132, | 0x76, 0xfd, | 0x8e, 0xff, | 0x58, 0x00 |
-984, | 178, | 121, | 0x70, 0xfd, | 0x89, 0xff, | 0x51, 0x00 |
-1002, | 195, | 112, | 0x64, 0xfd, | 0x7e, 0xff, | 0x4b, 0x00 |
-991, | 189, | 111, | 0x6b, 0xfd, | 0x82, 0xff, | 0x4a, 0x00 |
-990, | 193, | 108, | 0x6c, 0xfd, | 0x7f, 0xff, | 0x48, 0x00 |
-994, | 193, | 123, | 0x69, 0xfd, | 0x7f, 0xff, | 0x52, 0x00 |
-1003, | 187, | 32764, | 0x63, 0xfd, | 0x83, 0xff, | 0x00, 0x63 |
-994, | 192, | 106, | 0x69, 0xfd, | 0x80, 0xff, | 0x47, 0x00 |
-991, | 187, | 120, | 0x6b, 0xfd, | 0x83, 0xff, | 0x50, 0x00 |
-994, | 196, | 103, | 0x69, 0xfd, | 0x7d, 0xff, | 0x45, 0x00 |
-999, | 192, | 109, | 0x66, 0xfd, | 0x80, 0xff, | 0x49, 0x00 |
-1003, | 193, | 108, | 0x63, 0xfd, | 0x7f, 0xff, | 0x48, 0x00 |
-997, | 198, | 105, | 0x67, 0xfd, | 0x7c, 0xff, | 0x46, 0x00 |
------------------------------------------------------------------|
-993, | 195, | 118, | 0x6a, 0xfd, | 0x7e, 0xff, | 0x4f, 0x00 |
-993, | 195, | 123, | 0x6a, 0xfd, | 0x7e, 0xff, | 0x52, 0x00 |
-991, | 180, | 114, | 0x6b, 0xfd, | 0x88, 0xff, | 0x4c, 0x00 |
-987, | 193, | 121, | 0x6e, 0xfd, | 0x7f, 0xff, | 0x51, 0x00 |
-1003, | 183, | 118, | 0x63, 0xfd, | 0x86, 0xff, | 0x4f, 0x00 |
-991, | 192, | 32764, | 0x6b, 0xfd, | 0x80, 0xff, | 0x50, 0x6b |
-982, | 190, | 126, | 0x71, 0xfd, | 0x81, 0xff, | 0x54, 0x00 |
-1000, | 192, | 124, | 0x65, 0xfd, | 0x80, 0xff, | 0x53, 0x00 |
-996, | 187, | 120, | 0x68, 0xfd, | 0x83, 0xff, | 0x50, 0x00 |
-996, | 189, | 118, | 0x68, 0xfd, | 0x82, 0xff, | 0x4f, 0x00 |
-999, | 196, | 121, | 0x66, 0xfd, | 0x7d, 0xff, | 0x51, 0x00 |
-994, | 190, | 114, | 0x69, 0xfd, | 0x81, 0xff, | 0x4c, 0x00 |
-------|--------|--------|-------------|-------------|------------|
-1000, | 192, | 121, | 0x65, 0xfd, | 0x80, 0xff, | 0x51, 0x00 |
-996, | 196, | 120, | 0x68, 0xfd, | 0x7d, 0xff, | 0x50, 0x00 |
-993, | 190, | 127, | 0x6a, 0xfd, | 0x81, 0xff, | 0x55, 0x00 |
-996, | 181, | 120, | 0x68, 0xfd, | 0x87, 0xff, | 0x50, 0x00 |
-997, | 186, | 32764, | 0x67, 0xfd, | 0x84, 0xff, | 0x00, 0x67 |
-996, | 186, | 126, | 0x68, 0xfd, | 0x84, 0xff, | 0x54, 0x00 |
-985, | 190, | 115, | 0x6f, 0xfd, | 0x81, 0xff, | 0x4d, 0x00 |
-991, | 193, | 120, | 0x6b, 0xfd, | 0x7f, 0xff, | 0x50, 0x00 |
-987, | 177, | 132, | 0x6e, 0xfd, | 0x8a, 0xff, | 0x58, 0x00 |
-969, | 172, | 139, | 0x7a, 0xfd, | 0x8d, 0xff, | 0x5d, 0x00 |
-985, | 177, | 130, | 0x6f, 0xfd, | 0x8a, 0xff, | 0x57, 0x00 |
2025-01-30 8:40 AM
Hi @amistar ,
You can read all the output registers. Can you implement our official drivers and let me know if you solve the issue?
Thanks
2025-01-31 3:15 AM
Hi
I found the problem, it was too high SPI frequency. According to info found in `stm32f7xx_hal_spi.c` file there are different limits of SPI frequencies, thus prescalers, depending on mode of operation used. We will switch to our own driver at some moment, but now sticking to 6.25 MHz instead of 10 MHz is good solution.
We have also another problem with HAL SPI, it does receive two bytes to much - below you can see a SPI transaction readout of axis X, Y, Z of magnetometer which receives 6 bytes, but SPI peripheral keeps clock working for another 2 bytes. We wont try to debug it, but rather switch to own SPI driver.
We can consider the problem solved
Best regards
2025-01-31 3:40 AM
Problem solved
I found similar topic: https://community.st.com/t5/stm32-mcus-products/stm32f767-spi-bidirectional-receive-mode-more-spi-clocks-are/m-p/213384#M46791
And this description why STM32HAL cant handle bidirectional SPI properly:
http://efton.sk/STM32/gotcha/g32.html
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.