2016-11-25 2:43 PM
I wish to filter incoming FIFO data by a threshold value as set in INT1_THS, however the WTM flag is set regardless of the magnitude. Are these two functions not compatible? If not, I need to know how to link the threshold setting to the FIFO data.
2016-11-30 5:01 AM
No, the functions are not compatible. Please check the datasheet for available FIFO modes.
If my understanding is correct, you want to store in FIFO only the data which are above a certain
threshold
, this is not possible.
The only available option is to use Stream-to-FIFO mode, it this mode the data are stored prior an interrupt. The
interrupt
can be configured to occur when
threshold
is reached.
Best regards
Miroslav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.