2018-08-19 11:36 PM
Hi,
I need to get the FIFO contents prior to impact, to do this, I enable high pass, and go to stream to FIFO mode. But I get an interrupt as soon as I finish configuring
I am configuring LIS2DH12 according to your application note:
CTRL_REG1 = 0x37 // 25Hz, xyz enabled
CTRL_REG2 = 0x0B // high pass data sent to FIFO and output regs
CTRL_REG3 = 0x01 // IA1 interrupt on INT1 pin
CTRL_REG4 = 0x48 // BDU, +-4g full scale reading
CTRL_REG5 = 0x0A // latch both interrupt pins
CTRL_REG6 = 0x14 // interrupt 2 on INT2 pin
INT1_THS = 0x0A // about 0.3g
INT1_DUR = 0x03
INT1_CFG = 0x2A // x high, or y high, or z high
FIFO_CTRL = 0x20 // trigger event allows triggering on INT2
CTRL_REG5 = 0x4A // enable FIFO
FIFO_CTRL = 0xE0 // set mode to stream to FIFO
Can you please take a look and tell me if I'm doing something wrong?
2018-08-20 1:04 AM
I see following problem:
CTRL_REG3 = 0x40 // IA1 interrupt on INT1 pin
CTRL_REG4 = 0x90 // BDU, +-4g full scale reading
CTRL_REG6 = 0x20 // interrupt 2 on INT2 pin
Then you configured to trigger the FIFO by INT2, but you configured the INT1 (INT1_THS, UNT1_DUR, INT1_CFG)!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.