2022-03-07 11:02 AM
Hi,
I was looking at LIS2DE12 and I am aware that it can send a wakeup signal to the CPU. In my design I want to enable the power on PMIC chip directly through its enable pin. So I want to do something like this:
I read about latching INT1 & INT2 in the specification paper but I am not sure this means this. I also found https://community.st.com/s/question/0D53W000012QA5NSAW/lis2de12-interrup-on-wakeup but I am not sure if the same case is described there.
Is it possible to make such operation? Just set some pin to 1 when wakeup is triggered and then reset it with another pin.
If this is not possible LIS2DE12 is there any other IC that works like this?
Thanks,
Matej
2022-03-11 6:57 AM
Hi Matej @Matej Šircelj ,
Yes, the procedure you are describing should be possible.
For this step:
in the latched interrupt case, you have to read the INT1_SRC (31h) register to clear the interrupt itself (see datasheet, p.21).
Only a remark: I suggest you to use a more recent part number than the LIS2DE12, such as the LIS2DW12, which is guaranteed for more years.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.