2016-07-02 10:07 PM
What is the maximum voltage of the L3G4200D INT1 pin (assuming open drain)?
What does the PP_OD bit in CTRL_REG3 control - INT1 only or INT1 and DRDY/INT2? What are the maximum voltages applied to all I/O pins? Why are ST's datasheets SO BAD? This part has been in production for 6 years. There's no excuse for not documenting it. #l3g4200d2016-07-14 1:02 AM
Maximum allowable voltage applied to the INT pins is Vdd_IO + 0.3V even if it is open-drain configuration.
I will ask expert.
Maximum allowable voltage applied to any I/O pin is Vdd_IO + 0.3V.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.