cancel
Showing results for 
Search instead for 
Did you mean: 

Is the iNEMO_DT(delta time) in iNEMO_Engine_Lite currect? or something wrong with it

gghyoo
Associate
Posted on October 25, 2011 at 11:48

Hi Fabio,

I find something confusing in the demo project.

The data update task is synchronized with the  Timer2 interrupt, and the timer2 is update every 0.02s(50Hz), so the delta time should be 0.02s. But the iNEMO_DT in iNEMO_Engine_Lite is set to 0.01. So something wrong with it, or I missed something.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.