cancel
Showing results for 
Search instead for 
Did you mean: 

iNEMO Engine M1 LI3 - ported to STM32F4 not showing coorect data

Bogdan
Senior
Posted on October 22, 2014 at 08:18

Hello, i am using the iNEMO Lite soft version, namely INEMOEngineM1LI3,

 the only thing i modified to work with the stm32f407 was some i2c functions, and the data/trafic on the i2c buss is ok.

I tryied to display the roll, pitch, and yaw on a 20x4 LCD display, and the Roll axis is ok, in the meaning that it moves from 0 - 180 -180 -0 ,

However the Pitch axis only moves from 0 to 88 degree, if i try to move above 88 degree its starts decending to 0 again

And the Yaw axis displays -121 degree, if i move the yaw axis the minimum value i can get is -60 degree

The header and source code is the same as in the

\INEMOEngineM1LI3\iNemo_M1_Applications\Source\examples\AHRS_Continuous.c

Is this a demo software limitation? Tryed even my own sensor libs and using inemo ahrs kalman filters and algorithms

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.