2020-12-14 12:25 AM
Also, are there libraries or example codes that we can use in our STM32 microcontroller, for specific applications like body movement detection ?
Solved! Go to Solution.
2020-12-14 4:31 AM
You are welcome, @LeoSandler
Understood...
>> Can the LSM6DSOX provide all these functions (Accel + Gyro), in addition to MLC ?
Yes of course on LSM6DSOX there are all the LSM6DS3 features and, and the FSM and MLC in addition.
-Eleon
2020-12-14 2:26 AM
Hi @LeoSandler ,
unfortunately, the LSM6DS3TR-C has not embedded machine learning core (MLC).
The sensors that have MLC embedded feature are the one that you can find at this link (or here for the accelerometers), and are marked with an "X" at the end of the product name. For example:
Let me please know if you need more support or, in case, please mark this answer as closed by selecting "Best Answer".
-Eleon
2020-12-14 2:37 AM
Thank you very much for your prompt answer.
The device we have currently in our design is LSM6DS3, which is NRND
I understood that the LSM6DS3TR-C is a direct replacement.
Since we want to add additional functionality to our device, without loosing the current one, I'm not sure if the LSM6DSOX is suitable.
With the LSM6DS3 we are using both Accelerometer and Gyro measurements.
Can the LSM6DSOX provide all these functions (Accel + Gyro), in addition to MLC ?
Thanks !
2020-12-14 4:31 AM
You are welcome, @LeoSandler
Understood...
>> Can the LSM6DSOX provide all these functions (Accel + Gyro), in addition to MLC ?
Yes of course on LSM6DSOX there are all the LSM6DS3 features and, and the FSM and MLC in addition.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.