2019-04-03 12:04 PM
The digital IO of pressure and temperature is nice, but we can also use an analog output. The digital is good for a new high volume project, but we need an analog output for a current application. Small size and low power requirements are also important as the instruments are portable and battery powered for extended periods.
Depending on the specific application, the environment exposes the sensor pressure input to sea water, industrial cooling water, and the stomach contents of cattle...rather a wide range but very challenging for an un-protected sensor.
2019-05-08 7:25 AM
Hi, unfortunately we have no such sensor in or catalog. however, you could theoretically encapsulate the sensor in a proper material to act as a force sensor and so increase the pressure full scale. But this is just a suggestion. Did you find a proper solution for your application in these weeks? Regards
2019-05-08 10:23 AM
No joy so far, but the one we have will work with the addition of a silicon oil barrier. Thanks for looking.
Kelly
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.