cancel
Showing results for 
Search instead for 
Did you mean: 

I guys, I was looking at the VL53L1X to detec water level in a manhole but it says the field of view is 15°-27°. Being in a manhole, this is way to wide. Any suggestions?

PGagn.1
Associate

The device I am developping on is on top of the manhole at 3-4 meters high and I need a 2-5 mm precision or so. I look forward for an idea. Looking at basic laser meters to take measurements, they all are capable of doing what I am looking for, but can't find what technology/sensor they use to make it happen... Any insight would be appreciated.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KnarfB
Super User

The sensor has 16x16 SPADs internally, see data sheet. Its possible to use parts of that downto 4x4. This will narrow the FoV.

Eleon BORLINI
ST Employee

Hi @PGagn.1​ , did you solved you issue?

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.