cancel
Showing results for 
Search instead for 
Did you mean: 

How to use AH_QVAR on STEVAL MKI250KA

Luisa_97
Associate II

Hi, I have STEVAL MKI109D, on it I mounted STEVAL MKI250KA. I would say if I could use QVAR Swipe Electrode mounted on STEVAL MKI250KA for reading Qvar signal. It is possible?

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Luisa_97 ,

Series capacitors CS1 and CS2 are used to remove DC voltage. By replacing these capacitors with a short, it can be used for UI applications (it is recommended to set the gain to 16x to ensure saturations).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
casadeib
ST Employee

Hi @Luisa_97 ,

In order to use QVAR Swipe electrode on STEVAL MKI250KA there are some modification that have to be implemented, otherwise for QVAR functionalities you can use MKI235KA.

Hope this could help.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @casadeib ,

Could you specify what modifications are required? I am usinf MKI235KA, but I would like to compare the signals recorded from both devices in MEMS-Studio to observe any differences. 

Thanks.

Hi @Luisa_97 ,

Series capacitors CS1 and CS2 are used to remove DC voltage. By replacing these capacitors with a short, it can be used for UI applications (it is recommended to set the gain to 16x to ensure saturations).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.