2018-06-04 6:13 AM
Hai, I want to build a data logger attached to an object travel at 3m/s. The requirement is the data logger must capture 74 sensor input (10 bit ADC) at every 3mm along the travel path. Thus in 1 second, the data logger must capture and save 3000 data per sensor and equivalent to 222 000 data for the whole 74 sensors.
I never exposed to this task before thus could you give an idea of the architecture of such system?.
#store-data #high-speedWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.