2020-11-23 6:14 PM
Hi,
I tried couple to run my code, but I can't just hear any noise or beep. I am very new to this.
One issue that I found is SPI3->DR is not receiving anything during debugging.
Here is my code and correct me,
#include <mbed.h>
#include<I2C.h>
#include <stm32f4xx_hal.h>
I2C i2c(PB_9,PB_6);
int main() {
//SETTING UP FOR SPI3
RCC->APB1ENR |= RCC_APB1ENR_SPI3EN; //Enable SPI3 clock
RCC->APB1RSTR |= (1<<15);//Reset the SPI3
RCC->APB1RSTR &= ~(1<<15);//Clear the SPI3
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOCEN;//Enable GPIO clock
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN;//Enable GPIO clock
int mclk_pinc=7,sclk_pinc=10,sd_pinc=12,fs_pina=4;//mclk_pin=7,sclk_pin=10,sd_pin=12,fs_pin=4;
const int slave_addr=0x94;
char sound_data[2];
// Configure I2S MCK, SCK, SD pins.
GPIOC->MODER &= ~(3UL<<(mclk_pinc*2));
GPIOC->MODER |= 2UL<<(mclk_pinc*2);
GPIOC->MODER &= ~(3UL<<(sclk_pinc*2));
GPIOC->MODER |= 2UL<<(sclk_pinc*2);
GPIOC->MODER &= ~(3UL<<(sd_pinc*2)); //sd_pin
GPIOC->MODER |= 2UL<<(sd_pinc*2);
GPIOA->MODER &= ~(3UL<<(fs_pina*2)); // lr clk
GPIOA->MODER |= 2UL<<(fs_pina*2);
GPIOE->OTYPER &=~(1<<mclk_pinc);
GPIOE->OTYPER &=~(1<<sclk_pinc);
GPIOE->OTYPER &=~(1<<sd_pinc);
GPIOA->OTYPER &=~(1<<fs_pina);
GPIOC->OSPEEDR |= (3<<(mclk_pinc*2));//High speed
GPIOC->OSPEEDR |= (3<<(sclk_pinc*2));//High speed
GPIOC->OSPEEDR |= (3<<(sd_pinc*2));//High speed
GPIOA->OSPEEDR |= (3<<(fs_pina*2));//High speed
GPIOC->PUPDR &=~(3UL<<(mclk_pinc*2));
GPIOC->PUPDR &=~(3UL<<(sclk_pinc*2));
GPIOC->PUPDR &=~(3UL<<(sd_pinc*2));
GPIOA->PUPDR &=~(3UL<<(fs_pina*2));
/* (appendix I of book) */
GPIOC->AFR[1] &= ~0xffffffff;//SPI3_SCK Serial Clock (mapped on the SCK pin)
GPIOC->AFR[1] |= 0x00000600;
GPIOC->AFR[1] &= ~0xffffffff;//SPI3_MOSI SD: Serial Data (mapped on the MOSI pin)
GPIOC->AFR[1] |= 0x00060000;
GPIOC->AFR[0] &= ~0xffffffff;//SPI3_MOSI SD: Serial Data (mapped on the MOSI pin)
GPIOC->AFR[0] |= 0x60000000;
GPIOA->AFR[0] &= ~0xffffffff;//SPI3_NSS WS: Word Select (mapped on the NSS pin)
GPIOA->AFR[0] |= 0x00060000;
// Configure CS43L22.
sound_data[0] =0x02;
sound_data[1] =0x01;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x04;
sound_data[1] =0xaf;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x05;
sound_data[1] =0x81;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x06;
sound_data[1] =0x04;
i2c.write(slave_addr,sound_data,2);
sound_data[0]=0x20;
sound_data[1]=90+0x19;
i2c.write(slave_addr,sound_data,2);
sound_data[0]=0x21;
sound_data[1]=90+0x19;
i2c.write(slave_addr,sound_data,2);
// Power on the code.
sound_data[0] =0x02;
sound_data[1] =0x9e;
i2c.write(slave_addr,sound_data,2);
// Configure codec for fast shutdown.
sound_data[0] =0x0a;
sound_data[1] =0x00;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x0e;
sound_data[1] =0x04;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x27;
sound_data[1] =0x00;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x1f;
sound_data[1] =0x0f;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x1a;
sound_data[1] =0x0a;
i2c.write(slave_addr,sound_data,2);
sound_data[0] =0x1b;
sound_data[1] =0x0a;
i2c.write(slave_addr,sound_data,2);
SPI3->I2SCFGR=0;// Disable I2S for configuration
// I2S clock configuration
RCC->CFGR&=~RCC_CFGR_I2SSRC; // PLLI2S clock used as I2S clock source.
RCC->PLLI2SCFGR=(50<<28)|(5<<6);
// Enable PLLI2S and wait until it is ready.
RCC->CR|=RCC_CR_PLLI2SON;
while(!(RCC->CR&RCC_CR_PLLI2SRDY));
// Configure I2S.
SPI3->I2SPR=1|(0<<8)|SPI_I2SPR_MCKOE;
SPI3->I2SCFGR=SPI_I2SCFGR_I2SMOD|SPI_I2SCFGR_I2SCFG_1|SPI_I2SCFGR_I2SE; // Master transmitter, Phillips mode, 16 bit values, clock polarity low, enable.
sound_data[0] =0x02;
sound_data[1] =0x9e;
i2c.write(slave_addr,sound_data,2);//Power on
while(1)
{
if((SPI3->SR & SPI_SR_TXE))
{
SPI3->DR = 0xffff; // This DR is not receiving anything.
}
}
}
2020-11-24 1:04 AM
If you ignore Cube/HAL anyway, I suggest to download the "old", SPL-based F4 Discovery firmware package, which contains drivers and example applications for the DAC.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.