2018-05-11 10:33 PM
Hello,
Unfortunately, I am having problems with the demo included in the X-CUBE-MEMSMIC1 package for the NUCLEO-L476RG. After loading the precompiled file to the board and attempting to plug it in to a computer via the X-NUCLEO-CCA02M1's connector, the device does not register with my computer (Linux or Windows). Can any troubleshooting advice be given?
I have not modified the jumpers on the board. Is my reading of the manual correct, and that I need to set the jumpers to DFSDM operation to use the pregenerated files (which as far as I can tell select DFSDM operation on the L476RG board)? Would this cause a failure to enumerate?
Thanks in advance!
#nucleo-l476rg #audio #microphoneWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.