cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am working with H3LIS331DLTR elements, I can not decipher the marking, can you help?

JRaim.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @JRaim.1​ ,

In addition to Peter's complete description, we can say the third line, and especially the two last letters/numbers, refer to the specific assembly lot of those samples.

This information is useful at failure analysis level.

-Eleon

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @JRaim.1​, to the community!

the important marking is H3D3, which stands for H3LIS331DLTR.

The first and last lines should only be required if a quality issue arises and the component would need to be examined in detail. Maybe the datecode here is interesting: line 1, 830 = year 2018, week 30.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JRaim.1
Associate II

Our quality engineers have encountered some problems in identifying the markings.

We would be very grateful if you could explain the meaning of the symbols (line 3) in the attached photo. Is it a data code or a lot number? How can one packing tape contain devices with different markings?

Hi @JRaim.1​ ,

In addition to Peter's complete description, we can say the third line, and especially the two last letters/numbers, refer to the specific assembly lot of those samples.

This information is useful at failure analysis level.

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.