2020-10-13 4:43 AM
Hi,
our customer is in search for a economical solution for a gadget posistion sensor, that senses 2 positions: the gadget is in standing or in laying positions. What can we suggest?
Solved! Go to Solution.
2020-10-13 6:08 AM
Hi @Dmitry Vasilenko ,
Since the target application is a gadget, I believe it should consume as little power as possible. So, I would suggest the LIS2DW12 ultra-low-power high-performance three-axis linear accelerometer, which has the embedded 6D/4D orientation digital feature, described in the datasheet and in the AN5038 application note at p. 23.
You can also refer to the C example repository on Github for the code implementation of this feature --> lis2dw12_orientation.c.
-Eleon
2020-10-13 6:08 AM
Hi @Dmitry Vasilenko ,
Since the target application is a gadget, I believe it should consume as little power as possible. So, I would suggest the LIS2DW12 ultra-low-power high-performance three-axis linear accelerometer, which has the embedded 6D/4D orientation digital feature, described in the datasheet and in the AN5038 application note at p. 23.
You can also refer to the C example repository on Github for the code implementation of this feature --> lis2dw12_orientation.c.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.