cancel
Showing results for 
Search instead for 
Did you mean: 

Does LSM303 has high sensing range than the bosch BMM150 sensor in terms of magnetic field range(x,y,z)(micro tesla)?

BRaj_48
Associate II

Have been working with magnetometers for the car parking application. the previous sensors used has not satisfied the range for the application required. Does LSM303 detect at a range of 30cms?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Eleon BORLINI
ST Employee

Hi @BRaj_48​ , as I can see from the BMM150 sensor datasheet, the magnetometer dynamic range is ±13 gauss on x and y axis and ±25 gauss along z axis, while the sensitivity is 3 mgauss/LSB. On the other hand, the LSM303AGR magnetometer part has a wider dynamic range (±50 gauss), while the minimum detectable signal is 1.5mgauss. The LSM303AGR capability is higher both in terms of Full Scale and resolution, so I believe that it can be cover your application requirements. Regards

BRaj_48
Associate II

Thank you for your time @Eleon BORLINI​, and i have an another doubt as which will have the capability to detect maximum distance is it milli-tesla or the micro-tesla(as the dynamic range)?

Should be some tenth of mT... Regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.