2022-08-03 9:34 AM
When we detect movement, we enable switch the LSM6DSOX into a fifo /w compression mode. We noticed we sometimes get a few "junk" entries of Gyro data in the beginning. Once we the a few entries into the system, the data looks good.
What is the correct sequence to setup the registers to avoid any glitches in the compressed fifo data stream?
For the data below, the device is on a turn table running at a relatively constant rate. The turn table is up to speed before the LSM6DSOX is enabled.
--- 2nd entry junk
W (11:05:42.883) IMU: 0A: 0x56 0xF3 0xFF 0x12 0x00 0x0D 0x00
W (11:05:42.885) IMU: 0A: 0x56 0x03 0x00 0x0C 0x00 0x08 0x00
W (11:05:42.890) IMU: 0A: 0x56 0xFA 0xFF 0x12 0x00 0x09 0x00
W (11:05:42.895) IMU: 0A: 0x56 0xFE 0xFF 0x0E 0x00 0x0B 0x00
--- 1st and 3rd entry junk
W (11:05:48.792) IMU: 0A: 0x53 0x00 0x00 0x4E 0x00 0xB7 0x00
W (11:05:48.793) IMU: 0A: 0x56 0xF8 0xFF 0x0F 0x00 0x1B 0x00
W (11:05:48.799) IMU: 0A: 0x56 0x00 0x00 0x10 0x00 0x0D 0x00
W (11:05:48.804) IMU: 0A: 0x56 0xFF 0xFF 0x12 0x00 0x09 0x00
--- 1st and 2nd entry junk
W (11:05:54.749) IMU: 0A: 0x53 0x00 0x00 0x4E 0x00 0xB7 0x00
W (11:05:54.750) IMU: 0A: 0x56 0x00 0x00 0x11 0x00 0x1C 0x00
W (11:05:54.756) IMU: 0A: 0x56 0xFF 0xFF 0x08 0x00 0x06 0x00
W (11:05:54.761) IMU: 0A: 0x56 0xFF 0xFF 0x0C 0x00 0x0E 0x00
--- good wakeup
W (11:08:17.908) IMU: 0A: 0x53 0x23 0xFE 0x8E 0xFD 0xF8 0xFA
W (11:08:17.909) IMU: 0A: 0x56 0xC6 0xFE 0x54 0xFD 0x11 0xFC
W (11:08:17.910) IMU: 0A: 0x53 0x99 0xFD 0x03 0xFC 0xAC 0xFA
W (11:08:17.922) IMU: 0A: 0x56 0xDD 0xFE 0xFD 0xFE 0xB9 0xF9
--- good wakeup
W (11:08:17.908) IMU: 0A: 0x53 0x23 0xFE 0x8E 0xFD 0xF8 0xFA
W (11:08:17.909) IMU: 0A: 0x56 0xC6 0xFE 0x54 0xFD 0x11 0xFC
W (11:08:17.910) IMU: 0A: 0x53 0x99 0xFD 0x03 0xFC 0xAC 0xFA
W (11:08:17.922) IMU: 0A: 0x56 0xDD 0xFE 0xFD 0xFE 0xB9 0xF9ctrl1_xl = ((4 - accelRate) << 4);
ctrl2_g = ((4 - gyroRate) << 4);
fifo_ctrl3 = ((4 - gyroRate) << 4) | (4 - accelRate);
imuMode = IMU_STATE_FIFO;
writeIMURegister(spiImu, FUNC_CFG_ACCESS, 0x00); // Switch to standard regs
writeIMURegister(spiImu, CTRL3_C, 0x01); // software reset
writeIMURegister(spiImu, CTRL9_XL, 0xE2); // disable I3C
writeIMURegister(spiImu, CTRL3_C, 0x44); // Block Data Update set
writeIMURegister(spiImu, CTRL1_XL, ctrl1_xl|0x0C); // Accelerometer sample rate, 8g
writeIMURegister(spiImu, CTRL2_G, ctrl2_g|0x04); // Gyroscope sample rate, 500 dps
writeIMURegister(spiImu, CTRL6_C, 0x10); // Acceleromter perf mode off
writeIMURegister(spiImu, CTRL7_G, 0x80); // Gyroscope perf more off
writeIMURegister(spiImu, FIFO_CTRL1, (FIFO_WATERMARK & 0xff)); //fifo watermark
writeIMURegister(spiImu, FIFO_CTRL2, 0x46 | ((FIFO_WATERMARK & 0x100) >>8)); //compression on, 32 batch rate, bit 9 of fifo watermark
writeIMURegister(spiImu, FIFO_CTRL3, fifo_ctrl3); // Gyroscope sample rate, Accelerometer sample rate
writeIMURegister(spiImu, FIFO_CTRL4, 0x06); //Continuous mode
writeIMURegister(spiImu, FUNC_CFG_ACCESS, 0x80); //Switch to embedded regs
writeIMURegister(spiImu, EMB_FUNC_EN_B, 0x08); //compression on
writeIMURegister(spiImu, EMB_FUNC_INIT_B, 0b0001000); // reset the FIFO compression algorithm
writeIMURegister(spiImu, FUNC_CFG_ACCESS, 0x00); //Switch to standard regs
writeIMURegister(spiImu, INT1_CTRL, 0x38); //INT1 on FIFO threshold
2022-08-05 5:31 AM
Hi @DFors.1 ,
Please have a look to the C example lsm6dsox_fifo_compressed.c on Github and compare your code with it.
You might try with lowering the ODR of the axl and the gyro, and check if you are still getting wrong samples, or adding an initial delay after the device wakeup.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.