2012-03-22 9:45 AM
Hello,
I am trying to get Data from several iNEMO2 MEMS using MatLab. My Code is the following: if not(libisloaded('lib')) [notfound, warnings] = loadlibrary('iNEMO2_SDK.dll', 'iNEMO2_SDK.h', 'alias', 'lib'); end Calling the functions libisloaded('lib') afterwards, returns a 1, so the libary has been loaded. I also can see the functions I am able to use. The COMPort the device is connected to is: 3 The Sensor reacts on using the iNEMO Suite 2.0. If I try to connect to the sensor using MatLab as follows: sCOMa = strcat('PL=PL_001{PN=COM', 3, ',SENDMODE=B}'); [handle_devA] = calllib('lib', 'INEMO2_Connect', sCOMa); con = calllib('lib', 'INEMO2_IsConnect', handle_devA) the variable 'con' is set 0. So the device is not connected and I do not get any Data. I do the same procedure for several iNEMO Devices, giving each Device another handler and connect to another COMPort. Are the commands and parameters I use to establish the connection correct? I hope someone can help me solving my problem. Thanking you in anticipation!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.