2013-06-24 10:58 AM
Hi,
I am trying to configure LIS3DH in FIFO/Stream mode and have a few questions as the data sheet is not very clear.1) Can I configure the INT2 as the WaterMark interrupt? I don't see any option to configure INT2 as the interrupt in the register bits, although the spec seems to imply it is possible. Our hardware has the INT2 pin connected to a GPIO, hence would like to know if configuring INT2 as the watermark interrupt is an option.2) Since I couldn't configure INT2, I went with polling the WTM bit of FIFO_SRC_REG to see if the watermark threshold level has reached (assuming WTM bit is the place to look for). However, whenever I read FIFO_SRC_REG it comes out as 0. I have enabled the FIFO in CTRL_REG5 (bit 6) and set the mode in FIFO_CTRL_REG. What am I missing? Also, FIFO_SRC_REG doesn't have any explanation on what the reg bits mean.2013-06-24 12:52 PM
Quick correction on point 2.
However, whenever I read FIFO_SRC_REG it comes out as 0x20 (not 0 as mentioned before). FIFO seems to be empty.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.