2017-12-28 1:11 AM
I have this
http://www.kynix.com/Parts/3294011/SIT8009AC-11-18E-125.000000E.html
MEMS oscillator at 125MHz frequency (also the same with an OSC52 from SiWard at 25MHz) followed by a 1-to-4 clock driver to distrubute the clock to multiple ICs.When layouting, I always find myself asking what is the 'best' layout practices for them, since they are high speed signal sources and since I almost always have EMC problems related with these frequencies. This doesn't mean of course that the source of the problems are these oscillators. But I nevertheless look for ways to improve the layout at this corner.
Do you have any specific guidelines you follow when you layout such components?
Some of which I use are the following:
Do you have anything else to propose?
I want to share you with some useful articles:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.