2020-05-14 8:06 AM
I want to build a communications device that looks at 100-3000 psi pressures in my chemical plant and transmits the data to a receiver and GUI in the control room on a dedicated workstation. I am thinking it will take a .5-4.5 VDC pressure transducer, a ADC that will allow multiple pressure transducers to input and output. A controller that can manage the data transmits, and a WIFI transmitter.
On the receiving end, I am looking at a WIFI receiver and a controller that can convert the data and input it into a GUI.
I need help identifying what the exact parts I need are.
Can anyone help?
2020-05-15 4:17 AM
Hi @TMCGE.1 , I could suggest you to check the STWIN kit and especially its Wifi module, the STEVAL-STWINWFV1. The onboard module can be used together with the STWIN software, or it can be considered as stand alone: in this second could be a starting point to check the device specs and resources page. Btw, which cpecific kind of pressure sensor are you trying to configure? Regards
2020-05-15 5:59 AM
Thanks for the lead! I was looking into the following sensor for the cos and specs. Honeywell MLH08KPSB01A Industrial Pressure Sensor 8000 PSI .5-4.5 VDC OUT T122119
2020-05-30 3:15 AM
Don't call "anything wireless" a Wi-Fi, because Wi-Fi is a name of specific technology - IEEE 802.11 wireless networking. In your case it sounds like you need LoRa:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.