on 2025-02-19 6:27 AM
This article showcases the recently released STEVAL-MKI109D evaluation board, designed for all ST MEMS sensors. This evaluation board can be used to evaluate a sensor for a new application, analyze data from different sensors, and build and test a configuration for ST MEMS sensors. Users can thus develop context-aware applications with MEMS sensors more quickly, powerfully and flexibly.
The new STEVAL-MKI109D board is the new evaluation board for all ST MEMS sensors and it allows:
Figure 1: MEMS Studio - Sensor Evaluation, Line Charts
Figure 2: MEMS Studio - Sensor Evaluation, FFT
The STEVAL-MKI109D is the successor of the STEVAL-MKI109V3, and it continuously supports functionalities like:
Compared to the previous STEVAL-MKI109D generation, some additional features are available:
Figure 4: STEVAL-MKI109D
Figure 5: Connecting STEVAL-MKI109D to the PC through a USB type C cable
Figure 6: An SD-card slot is available on STEVAL-MKI109D
Plug an ST MEMS DIL24 adapter board on the STEVAL-MKI109D, as shown in the following figure. You can choose one among the large portfolio of adapters which ST offers for every sensor in production.
For example, here we use the STEVAL-MKI227KA DIL24 adapter board with the LSM6DSV16X.
Now MEMS-Studio and select STEVAL-MKI227KA (LSM6DSV16X) as the device name, shown in the picture below:
After selecting the device, click the start button to enable STEVAL-MKI109D to send data to the PC. Figure 9: MEMS Studio - Sensor Evaluation, quick setup
You can see the sensor outputs as numerical data and plots in MEMS-Studio.
Now, the following features are available:
Figure 12: MEMS Studio - Data Analysis, Time Domain
Figure 13: MEMS Studio - Data Analysis, Frequency Domain
Figure 14: MEMS Studio - Data Analysis, Spectrogram
Some of the advanced features available in MEMS-Studio for the new STEVAL-MKI109D are:
Figure 15: Sensor Fusion Low Power (SFLP) with STEVAL-MKI109D, STEVAL-MKI227KA and MEMS Studio
Figure 16: MEMS Studio - Advanced Features, FSM
Figure 17: MEMS Studio - Advanced Features, MLC
Figure 19: MEMS Studio - Advanced Features, ISPU Model Converter, Radar Chart
With a STEVAL-MKI109D and the MEMS-Studio software tool, you can speed up the evaluation for your application.
Now, it’s your turn, choose your sensor and start to design a new breakthrough application!
You can find STEVAL-MKI109D and the MEMS adapter boards on our eStore.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.