2017-06-07 12:11 AM
HI
We are planing to use a new WIFI module from ST for replacing the old module ( form another supplier )
so I :
1. bought a NUCLEO-F401RE and a X-NUCLEO.IDW04A boards.
2. downloaded the en.x-cube-wifi1_firmware software.
3. done the board setup according to page 6 in UM2183 (Getting started with the X-NUCLEO-IDW04A1)
4. compiled the firmware (Server_Socket) with IAR, and downloaded it to the board.
5. run.
and now the software get stuck in the wifi_reset() function wating for the stage to get started.
while(IO_status_flag.WiFi_WIND_State != WiFiHWStarted)
{ __NOP(); //nothing to do }so before I get started with the big investigation, I was thinking that maybe I wasn't the only one that have see this problem.
So I'm hoping that one of you guys can give me a hint, thanks in advance..
#x-cube-wifi1 #spwf04sa #x-nucleo-idw04a1Solved! Go to Solution.
2017-06-07 6:06 AM
Thanks, I found a solution:
- to use SW Reset functionality (wifi_reset() function)
- jumper on position JP3 (middle and top) is required (was not mounted)2017-06-07 5:02 AM
Hi,
By default, the build is set for SPWF04 and SPI interface. So if you are using UART as interface please set the required macros in the file wifi_conf.h in the Inc folder of the App you are running (e.g. server socket in your case).
Also check out the correct jumper settings for UART/SPI for the SPWF04 in the readme files.
IN case of UART it should be as below for the F401 board (not the comment out for SPWF01):
#ifdef USE_STM32F4XX_NUCLEO
#define CONSOLE_UART_ENABLED
//#define SPWF01
#define SPWF04
regards,
Mridu
2017-06-07 5:04 AM
you can also go through other threads discussing different versions of issues:
2017-06-07 6:06 AM
Thanks, I found a solution:
- to use SW Reset functionality (wifi_reset() function)
- jumper on position JP3 (middle and top) is required (was not mounted)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.