2017-05-15 1:53 AM
Now I am working with SP1ML(STEVAL-SP1ML868) and SPSGRF(X-NUCLEO-IDS01A4) modules working on 868 MHz frequency. SP1ML(USB Dongle) is connected to my MacBook where I can see what
SPSGRF is sending to me in
Putty software. SP1ML had astandard firmware, allowing AT commands to facilitate RF configuration, data transmission and reception, using simple point-to-point communication.
SPSGRF was programmed
using expansion software package . I have two problems with connection between my modules. First of all SPSGRF is sending to me very weird strings shown below:Below I have posted one more images showing the configurations of SP1ML module and code from Keil showing a configurations of SPSGRF module
. I checked: this is not problem with Baud Rate but I think it is problem with radio configuration. I also changed S28: PAYLOAD_SIZE to other value, but that didn't change anything.The second one is that I cannot send any data from SP1ML to SPSGRF.
Did anyone have a similiar problem?Tann.#wireless #spirit1 #spirit1-sp1ml #spsgrf #spiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.