2020-01-26 6:41 AM
Hi all,
Where can I find code example for STM32F429zi ram drive code
I see FatFS and other examples, but no ram-drive FatFS example
I need to open a device over USB to be recognized by the PC HOST
Thanks
Eli
2020-01-26 7:15 AM
I swear I posted an answer here.
I had written and posted an STM32F429I-DISCO SDRAMDISK back in the SPL days
For HAL/Cube you will probably need to find a MSC HOST for the EVAL boards, port to the DISCO, add SDRAM initialization, and change the IO to copy in/out of SDRAM
2020-01-26 7:18 AM
https://community.st.com/s/question/0D50X00009XkgpRSAR/using-stm32f429idiscovery-as-usb-otg-msc
2020-01-28 12:31 AM
Following me prev. question:
I am using STM32F429zi board
But found a RAM_DISK example for 9i board
I ran with / without RTOS
In both cases :
all these word fine (return woth OK :(
FATFS_LinkDriver, f_mount, f_mkfs,
But when I call f_open I get FR_NO_FILESYSTEM
How can that be ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.