2018-06-26 2:21 PM
Has anyone else encountered and solved a 'can't halt cpu' issue in IAR EWARM when using the segger j-link to program the BlueNRG-1 part through the 20 pin IDC jtag port on the STEVAL-IDB007V2? If so could you share the fix?
I can read and flash the BlueNRG-1 through J-Link commander but that's not a good debug environment. I also have a couple of ST-Link v2s here but those throw errors claiming inability to connect to the CPU.
With the J-link IAR's debug log is as follows:
Tue Jun 26, 2018 17:10:39: IAR Embedded Workbench 8.20.2 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\bin\armproc.dll)
Tue Jun 26, 2018 17:10:40: JLINK command: ProjectFile = C:\Users\hgoldstein\Documents\ST\BlueNRG-1_V1 DK 1.0.0\Project\BLE_Examples\BLE_Chat\EWARM\settings\BLE_Chat_Client.jlink, return = 0 Tue Jun 26, 2018 17:10:40: Device 'BLUENRG1' selected. Tue Jun 26, 2018 17:10:40: Selecting SWD as current target interface. Tue Jun 26, 2018 17:10:40: JTAG speed is fixed to: 1000 kHz Tue Jun 26, 2018 17:10:40: Found SW-DP with ID 0x0BB11477 Tue Jun 26, 2018 17:10:40: Scanning AP map to find all available APs Tue Jun 26, 2018 17:10:40: AP[1]: Stopped AP scan as end of AP map has been reached Tue Jun 26, 2018 17:10:40: AP[0]: AHB-AP (IDR: 0x04770021) Tue Jun 26, 2018 17:10:40: Iterating through AP map to find AHB-AP to use Tue Jun 26, 2018 17:10:40: AP[0]: Core found Tue Jun 26, 2018 17:10:40: AP[0]: AHB-AP ROM base: 0xE00FF000 Tue Jun 26, 2018 17:10:40: CPUID register: 0x410CC200. Implementer code: 0x41 (ARM) Tue Jun 26, 2018 17:10:40: Found Cortex-M0 r0p0, Little endian. Tue Jun 26, 2018 17:10:40: FPUnit: 2 code (BP) slots and 0 literal slots Tue Jun 26, 2018 17:10:40: CoreSight components: Tue Jun 26, 2018 17:10:40: ROMTbl[0] @ E00FF000 Tue Jun 26, 2018 17:10:40: ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB008 SCS Tue Jun 26, 2018 17:10:41: ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 000BB00A DWT Tue Jun 26, 2018 17:10:41: ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 000BB00B FPB Tue Jun 26, 2018 17:10:41: Executing ResetTarget() Tue Jun 26, 2018 17:10:42: BL reset: Timeout while waiting for CPU to halt after reset. Manually halting CPU. Tue Jun 26, 2018 17:10:42: Warning: CPU could not be halted Tue Jun 26, 2018 17:10:42: Hardware reset with strategy 0 was performed Tue Jun 26, 2018 17:10:42: Initial reset was performed Tue Jun 26, 2018 17:10:59: Executing ResetTarget() Tue Jun 26, 2018 17:10:59: BL reset: No application found. Manually halting CPU. Tue Jun 26, 2018 17:10:59: Warning: CPU could not be halted Tue Jun 26, 2018 17:10:59: Hardware reset with strategy 0 was performed Tue Jun 26, 2018 17:10:59: Initial reset was performed Tue Jun 26, 2018 17:11:05: IAR Embedded Workbench 8.20.2 (C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.0\arm\bin\armproc.dll)I tried most of the reset options with the same results. Thanks!
#bluenrg-1 #segger #iar #st-link #ewarm #j-link2018-06-27 1:09 AM
Hi Howard,
do you have any STM32 Nucleo board? If yes, you could use the embedded ST-LINK/V2-1 of your Nucleo by means of the SWD pins.
Best regards,
Antonio
2018-06-27 12:53 PM
Hello Antonio, thanks for your reply. I'll try a Nucleo if I run into the issue again. A workaround that got me running involved holding down the eval board's reset button and releasing it just as I depressed the program-flash button on IAR's IDE. It took 5 or 10 tries but eventually I timed it correctly and wound up at a dialog complaining that the part was protected and asking if I wanted to mass erase it. I saved off the flash contents before allowing the mass erase and afterwards I can now program and debug the bluenrg-1.
2018-06-27 8:33 PM
Hi Howard,
Could you please try to
force IO7 pin high during HW resetting the device?
It sounds like you were seeing some situation where SWD cannot be accessed when:
application that set the device in sleep or standby state, which the debug port (SWD) is not powered.
Thank you.
Best Regards,
Winfred
2018-06-28 8:28 AM
Thank you WInfred, in that I've flashed this puppy a half dozen more times since I first had the issue and it didn't crop up again your diagnosis sounds spot-on. Around mid-summer I expect to be told to develop a battery powered device and expect I'll have a chance to use your solution to flash it. Best Regards, Howard
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.