2023-10-26 10:20 AM
Hi,
I'm working on Power Line Communication with ST8500, with evaluation board equipped with STM32G0 and ST8500.
I'm able to send and receive UDP messages between 2 nodes, but I'd like to implement the IPV6 multicast feature. In particular, I want that one specific node send UDP datagram to all the nodes of the network.
Multicast came into my mind, but I don't think it is implemented.
Is there a way to do so?
Regards,
2023-11-23 2:29 AM
Dear user,
I can invite you to download the latest package version available on st.com. it is called STSW-ST8500GH-2. It integrates IPv6 multicast functionality. This package is made for the new EVLKST8500GH-2 but it can also be adapted to be compatible with the previous EVLKST8500GH868 and EVLKST8500GH915 kits by re-mapping its pinout. Or you can just have a look on it to see how the multicast is handle.
To give you some information about the multicast implementation. Multicast means that the devices are registered to a multicast group. By default all the devices are added in the group 0x8001 and 0x8002. So to send a UDP datagram to these multicast groups you need to use these IPv6 addresses respectively: F020000000000000000000000000001 and F020000000000000000000000000002 as the destination address. The devices should receive the indication message.
Make sure also that the connection ID is well configured.
Best regards,
Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.