2020-11-24 6:45 AM
I'd like to use the ST202/ST232 as a drop in replacement for MAX202/MAX232 devices.
In my design, the V+ output is connected to GND (via capacitor) as suggested in the datasheet
https://www.ti.com/lit/ds/symlink/max232.pdf
Whereas the ST datasheet
https://www.st.com/resource/en/datasheet/st202eb.pdf
has V+ output connect to VCC (via capacitor).
Does the ST202/ST232 also allow for V+ to be connected to GND (via capacitor) or is is better to adhere to the application example? In other words, can I use the ST device as a drop in replacement or do I have to redesign?
Thanks a lot.
Dan
2020-12-18 1:57 AM
Received an answer from ST support:
"We confirm the ST component can be used. Connection of C3 to GND or VCC doesn’t impact the behavior."
C3 is the capacitor connected to V+ according to ST's datasheet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.