2017-05-11 6:04 AM
Hi!
I am using the SPWF04SA module. I am trying to create dynamic pages. My webpage is done and it works. I'm having problems with updating the tokens buffer using the AT+S.INPUTSSI command as described in the AN4965 Application note and UM2114 User Manual.
The problem is, if I send more than 255 bytes with AT+S.INPUTSSI command, the module became unresponsive! No more AT commands are recognized, and after 20 seconds the Watchdog resets the module. I think this is a bug, and if the SSI tokens buffer is limited to 255 bytes, this should be mentioned in the manual and/or application note.
So, when I send this:
AT+S.INPUTSSI=256
|{1111;11/05/2017;16:00}|{1111;11/05/2017;16:00;0;1;11,00;116;0;0}|{1111;11/05/2017;16:00;116;0;0;0;6;0;0}|{1111;11/05/2017;16:00;7;1;0;2;1;0;12345;0.0.0.0;123456789012345;1234567890123456}|{1111;11/05/2017;16:00;22:32:43;33;3;8;19:42:43;32;2;65}|{012345}|I get no answer from the module, and I have to wait 20 seconds for the watchdog to reset the module.
Instead if I send this:
AT+S.INPUTSSI=255
|{1111;11/05/2017;16:00}|{1111;11/05/2017;16:00;0;1;11,00;116;0;0}|{1111;11/05/2017;16:00;116;0;0;0;6;0;0}|{1111;11/05/2017;16:00;7;1;0;2;1;0;12345;0.0.0.0;123456789012345;1234567890123456}|{1111;11/05/2017;16:00;22:32:43;33;3;8;19:42:43;32;2;65}|{01234}|I get answer and everything is ok.
So, the question: is this a bug, or the tokens buffer are limited to 255. Even if the tokens buffer are limited to 255, this is a bug, because the module is completely blocked until the watchdog reset...
I hope you have a solution for this, because we are migrating from SPWF01S to this new module, and I really need dynamic pages for more than 255 bytes.
Thank you
2017-05-12 1:55 AM
Hi,
thanks for feedback. There is a bug on tokenizer (mismatch on u8/u16 type) on FW1.0.0. Fixed, and available on near coming FW1.1.0 (a few weeks) currently under testing.
No constraints about the number of tokens, or length.
With fix:
12-May-17 10:54:51 [TX] - AT+S.INPUTSSI=256<CR>
|{1111;11/05/2017;16:00}|{1111;11/05/2017;16:00;0;1;11,00;116;0;0}|{1111;11/05/2017;16:00;116;0;0;0;6;0;0}|{1111;11/05/2017;16:00;7;1;0;2;1;0;12345;0.0.0.0;123456789012345;1234567890123456}|{1111;11/05/2017;16:00;22:32:43;33;3;8;19:42:43;32;2;65}|{012345}|12-May-17 10:54:51 [RX] - AT+S.INPUTSSI=256<CR><LF>AT-S.Managing Tokens:6<CR><LF>AT-S.OK<CR><LF>Thanks again
Ciao
jerry
2017-05-17 1:56 AM
Thank you for the answer Gerardo. I would like to ask you if it is possible to give me FW with this bug fixed, so we can go on with our development.
Anyway, I think I found another bug/limitation, now on the POST side...
The POST request is limited to 64 bytes, so I cannot send more than 64 bytes with a POST...If I send 65 bytes, the last byte is truncated and only 64 bytes are delivered by the module. 64 bytes for a POST are not enough...
I am looking forward for your answer.
Thank you
2017-05-17 5:04 AM
Ciao Tibor,
are you talking about the output demo (the 'opposite' of input SSI)?
jerry
2017-05-17 5:32 AM
Yes, I am talking about output_demo.html.
I send this from browser (using POST output_demo.html): Output=SetNetSet{6;1;0;2;1;0;172.10.20.1;123456789012345;123456789012345678}
There are 68 bytes of data in the above request.
The module outputs this on uart console: +WIND:57:Output from remote:64:SetNetSet{6;1;0;2;1;0;172.10.20.1;123456789012345;123456789012345
The module outputs only 64 bytes, but the request contains 68 bytes...
Thanks,
Tibor
2017-05-17 7:11 AM
Please open a new thread.
I think this will be a typical question in the future, and maybe other people can find this helpful. I will give you a reply in the new thread
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.