2021-05-09 12:15 PM
Hi,
I try to establish a connection between the SPIRIT1 radio on B-L475E-IOT01A board and the S2LP radio on the STEVAL-FKI868V1 evk. I found the library supporting both modules (STM32CubeExpansion_SUBG1) and managed to configure both modems. The problem is that after identical radio and packet configuration with 2-FSK modulation I still failed to send any data packed from the S2LP to SPIRIT1. The only thing that the SPIRIT1 radio receives is the recognized carrier. It fails to recognize the preamble and sync bytes. So I would like to ask if it is possible to communicate between these two modems? I understand that with identical radio parameters it should work. Maybe there is some working example that I could use as a base for my application?
Best regards,
Krzysztof
2021-09-15 8:07 AM
Hello Krzysztof,
The reason why the two modules are not interoperating might be that P2P configuration running on SPIRIT1 is using a packet length field of 7 bits while the S2LP uses 8 bit (standard). With below, SPIRIT1 packet length will change to 8 bits.
File : SPIRIT_PktBasic.c
Function: void SpiritPktBasicInit(PktBasicInit* pxPktBasicInit)
tempRegValue[1] = ((uint8_t) PCKTCTRL3_PCKT_FRMT_BASIC) | ((uint8_t)(pxPktBasicInit->cPktLengthWidth-1));
Change to
tempRegValue[1] = ((uint8_t) PCKTCTRL3_PCKT_FRMT_BASIC) | ((uint8_t)(pxPktBasicInit->cPktLengthWidth));
Hope this helps,
Marco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.