2022-07-06 4:45 AM
Dear ST Community,
I have the following test setup:
- 1x SPIRIT-1 transmitter (reads a pin from a STM32 MCU and modulates it over the radio)
- 2x SPIRIT-1 receivers (receive the pin state and pass it to the MCU)
Expectation: Both receivers should receive the same bit-stream data, sent by the transmitter.
Now.. whenever I use a single receiver (either #1 or #2 only), everything works fine every time after restart. However, as soon as I start the second receiver, it somehow does not receive the data. After numerous restarts I have observe the following sporadic behavior:
- Receiver #1 works, Receiver #2 does not
- Receiver #2 works, Receiver #1 does not
- Occasionally and rarely, both Receiver #1 and #2 work
I expect that since I am using a single pin for data transmission, I have properly bypassed the framing subsystem. So... is it related to some "negotiation" procedure, like on-boot CRC polynomial generation or anything similar? May someone suggest what I may be missing?
Thanks and regards!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.