2019-09-20 7:36 AM
2019-09-22 8:11 PM
As you've already noticed:
in_buffer[0] : 0 = Write, 1 = Read, 0x80 = Command
in_buffer[1] : Register Address or Command
in_buffer[2 ~ n_bytes-1] : Data
Sometimes it is also used for raw data feeding into FIFO, in this case, the whole buffer contains data.
2019-09-25 9:39 AM
I'm just integration via difference MCU. but, still have problem of tht "5.6.2 Transmitter data modes - Direct through FIFO mode". Register setting "#define PCKTCTRL1_ADDR ((uint8_t)0x30)" Value is 0x04.
Your reference design source using write below two FIFO data via S2LPSpiRaw function.
0,FF,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0
0,FF,0,56,0,4C,0,49,0,42,0,39,0,33,0,2E,0,29,0,25,0,20,0,1E,0,1C,0,1A,0,18,
0,17,0,16,0,15,0,13,0,13,0,11,0,11,0,10,0,10,0,F,0,F,0,E,0,E,0,D,0,D,0,D,0,
D,0,C,0,C,0,C,0,C,0,C,0,B,0,B,0,B,0,B
Our using general FIFO access method
0,FF, ==> FIFO Write Command
0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0 ==> Data Write
0,FF, ==> FIFI Write Command
0,56,0,4C,0,49,0,42,0,39,0,33,0,2E,0,29,0,25,0,20,0,1E,0,1C,0,1A,0,18,
0,17,0,16,0,15,0,13,0,13,0,11,0,11,0,10,0,10,0,F,0,F,0,E,0,E,0,D,0,D,0,D,0,
D,0,C,0,C,0,C,0,C,0,C,0,B,0,B,0,B,0,B ==> Data Write
after send to TX Command result to "IRQ_TX_FIFO_ERROR".
Could please let me know what is difference FIFO function method.
Thanks
2019-09-25 4:22 PM
HI ST Micro Team
I have more trying coding for "S2LPSpiRaw" function. but, It is same result for "IRQ_LOW_BATT_LVL".
Also, Our Reference Design H/W via "X-NUCLEO-S2915A1" and reference source is "BLE-Sub1GHz DK_2.0.0"
The difference between this is the front end module (SKY66420 vs SKY66431).
Please let us know about this issue and any advice.
static void priv_ST_MANUF_rf_load_first_ramp_up()
-----
/* fill the 1st part of the FIFO */
priv_ST_MANUF_SpiRaw_Ramp(18, (uint8_t*)zeroes, NULL,0);
priv_ST_MANUF_SpiRaw_Ramp(82, (uint8_t*)st_manuf_context->bpsk_ramps->fifo_start_ramp_up_1, NULL,0)
SPI FIFO WRITE DATA
E: ## S2LPSpiRaw ## n_butes= 12, can_return but = 0
E: [0, FF, 0, 0, 0]
E: WR DATA : [0,ff,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,]
E: SF_LIB : priv_ST_MANUF_SpiRaw_Ramp pwr_reduction:[0]
V: =====================================================================
E: ## S2LPSpiRaw ## n_butes= 52, can_return but = 0
E: [0, FF, 0, 56, 0]
E: WR DATA : [0,ff,0,56,0,4c,0,49,0,42,0,39,0,33,0,2e,0,29,0,25,0,20,0,1e,0,1c,0,1a,0,18,0,17,0,16,0,15,0,13,0,13,0,11,0,11,0,10,0,10,0,f,0,f,0,e,0,e,0,d,0,d,0,d,0,d,0,c,0,c,0,c,0,c,0,c,0,b,0,b,0,b,0,b,]
V: =====================================================================
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.