2015-10-04 5:38 PM
I'm wanting to load a custom firmware onto the SP1ML-915, as I'd like to implement abilities I can't get through the existing AT command set.
Where can I find documentation about how the STM32L151RB is connected to the Spirit1 chip? i.e. which spi on what pins? Also, does STM32CubeMX offer any help in setting up a base for a this type of firmware? Would appreciate any pointers, as I'm fairly new to all of this.2015-12-27 8:26 PM
I'm also interested about the possible answers to this question.
That would be a huge benefit to use the stm32 inside the module for our own application (gather some simple acquisitions from a sensor) rather that including another mcu only for that purpose. Thank you. Alex2016-02-04 1:58 PM
Simply use the P2P example included in STM32CubeExpansion_SUBG1_V1.0.0.
Then you should know that:PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISOPA4 ------> SPI1_NSSPA7 ------> SPI1_MOSIPA1 ------> SPIRIT_SDN
PC4 ------> SPIRIT_IRQ0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.