2017-11-04 11:07 AM
Hi
I received 2 of this kit, and I ran some basic tests - works really fine!
I am trying to use S2-LP in wm-bus solution for my project. I have a question regarding redudcing the capacitors/inductors count on the PCB : is there any chance to use balun (say with a freq range of
850MHz ~ 915MHz
(
) ? And if yes, how would that change the circuit ?Thanks in advance!!
Silas
#s2-lp2017-11-07 8:43 AM
Hi Silas,
Good to hear that you are using S2LP device.
We are currently integrating the Balue (BALF-SPI2-01D3) with S2-LP and making new Nucleo expansion board. We are validating the first prototype. S2LP package will be available on ST.com by end of Q4 or early Q1.
Meanwhile, please referrer the piece of schematic below which may be useful for you.
BR,
Indar
________________ Attachments : S2LP_with_Balun.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyKa&d=%2Fa%2F0X0000000b66%2FLsGvNaOulQR1uhS_EJ52xAqzQwqmm0_bbKrelrOmIHI&asPdf=false2017-11-07 4:31 PM
Hi Indar,
Thank you so much for your reply and the schematic with balun, this really reduces the component count and simplifies the design!
Well, further looking up more information on this particular balun you mentioned, it seems this is an ST product and specifically customized for S2-LP !!!! Wonderful!! And the data sheet is also available (
) with the schematic!! I am sure the schematic must have been tested.One more question:
Can we do this schematic on two-layer pcb? Or do I need to do 4 layer?
Thanks again,
Silas
2017-11-11 12:26 PM
Hi Indar,
For the reference data sheet ofBALF-SPI2-01D3
(
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fdatasheet%2Fgroup3%2Fe9%2Fff%2Fcd%2F1e%2F4f%2Fdd%2F49%2Fb4%2FDM00417488%2Ffiles%2FDM004174pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM004174pdf
)would you please help for some clarifications:
1In the schematic in figure 9, there is reference to jumpers JP1 to JP5, but is no such jumper in the schematic.. would you please provide some information on this?
2. The reference data sheet is marked with date 'Aug 2017' at the bottom on the first page, is there any updated version of this reference data sheet? Would you please help. ..
Thanks again
Silas
2017-11-13 10:36 PM
Hello Indar
Will you please provide any update on the above..?
Thanks
Silas
2017-11-21 7:14 PM
Hello
Anyone has worked with this balun (
BALF-SPI2-01D3) with S2-LP? I would really appreciate any information on the schematic given in the datasheet of the balun. I am planning on using S2-LP and possibly with this balun.
Thanks in advance!!
Silas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.