2020-03-19 11:21 AM
Hi, I am using cubemx to configure a stm32f411ve board as slave in receive only, polling mode and sofware NSS, in the code generated I have only added a few lines of code, only which I consider neccesary
**the master sends 12 bytes
outside main function:
uint8_t rxbuffer[12];
void Timeout_Error_Handler()
{
while(1){
HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_13); //led orange
HAL_Delay(500);
}
}
void Error_Handler2()
{
HAL_GPIO_WritePin(GPIOD,GPIO_PIN_14,GPIO_PIN_SET); //led red
}inside main function:
// I have commented the while (1) because for my test the master sends data just one time
//while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
switch (HAL_SPI_Receive(&hspi5,rxbuffer,12,5000))
{
case HAL_OK:
/* Turn LED6 on: Transfer in reception process is correct */
HAL_GPIO_WritePin(GPIOD,GPIO_PIN_15,GPIO_PIN_SET); //led blue
break;
case HAL_TIMEOUT:
Timeout_Error_Handler();
break;
case HAL_ERROR:
Error_Handler2();
break;
default:
break;
}the issue is that I am receiving only 0XFF
I was testing the same board with the slave code provided by ST in the stm32f411 examples:
STM32Cube\Repository\STM32Cube_FW_F4_V1.25.0\Projects\STM32F411E-Discovery\Examples\SPI\SPI_FullDuplex_ComPolling
and this code works ok BUT I want to implement hardware slave select, this example uses the SPI2 of the board and that SPI does not allow to configure a hardware slave select, so I thought the easiest way to achieve this was create a new project with other SPI peripheral of the board (I am using SPI5) and include the hardware slave select option (once I have tested that without this option works ok, as the example provided by ST)
is there any configuration function I am missing?
thanks
2020-03-19 1:10 PM
If HAL_SPI_Receive returns HAL_OK, then it's reading something. Likely the MOSI signal isn't making it to you somehow.
Check your pin assignments and AF selection of those pins.
Verify the signal actually exists using a scope or logic analyzer.
2020-03-19 1:30 PM
The pins are configured as default by the cubemx:
I dont have a logic analyzer right now
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.