2019-02-18 3:03 AM
My project is based on the END_NODE project provided by ST.
In a first time I fixed the Data rate to DR_4 for my payload need.
Now i want to try to use the ADR protocol.
So i change from
* LoRaWAN Adaptive Data Rate
* @note Please note that when ADR is enabled the end-device should be static
*/
#define LORAWAN_ADR_STATE LORAWAN_ADR_OFF
/*!
* LoRaWAN Default data Rate Data Rate
* @note Please note that LORAWAN_DEFAULT_DATA_RATE is used only when ADR is disabled
*/
#define LORAWAN_DEFAULT_DATA_RATE DR_4to
* LoRaWAN Adaptive Data Rate
* @note Please note that when ADR is enabled the end-device should be static
*/
#define LORAWAN_ADR_STATE LORAWAN_ADR_ON
/*!
* LoRaWAN Default data Rate Data Rate
* @note Please note that LORAWAN_DEFAULT_DATA_RATE is used only when ADR is disabled
*/
#define LORAWAN_DEFAULT_DATA_RATE DR_0But I see nothing activated by the ADR...
I'm on the thing network server.
The only change is in the lora.c files here
mibReq.Type = MIB_ADR;
mibReq.Param.AdrEnable = LoRaParamInit->AdrEnable;
LoRaMacMibSetRequestConfirm( &mibReq );Any idea?
I read these two links :
https://community.st.com/s/question/0D50X00009XkbSMSAZ/icubelrwan-v112-set-tx-power?t=1550487240182
https://www.thethingsnetwork.org/docs/lorawan/adr.html
EDIT :
I found this in loramac.c
/*!
* LoRaMAC MCPS-Request for a confirmed frame
*/
typedef struct sMcpsReqConfirmed
{
/*!
* Frame port field. Must be set if the payload is not empty. Use the
* application specific frame port values: [1...223]
*
* LoRaWAN Specification V1.0.2, chapter 4.3.2
*/
uint8_t fPort;
/*!
* Pointer to the buffer of the frame payload
*/
void* fBuffer;
/*!
* Size of the frame payload
*/
uint16_t fBufferSize;
/*!
* Uplink datarate, if ADR is off
*/
int8_t Datarate;
/*!
* Number of trials to transmit the frame, if the LoRaMAC layer did not
* receive an acknowledgment. The MAC performs a datarate adaptation,
* according to the LoRaWAN Specification V1.0.2, chapter 18.4, according
* to the following table:
*
* Transmission nb | Data Rate
* ----------------|-----------
* 1 (first) | DR
* 2 | DR
* 3 | max(DR-1,0)
* 4 | max(DR-1,0)
* 5 | max(DR-2,0)
* 6 | max(DR-2,0)
* 7 | max(DR-3,0)
* 8 | max(DR-3,0)
*
* Note, that if NbTrials is set to 1 or 2, the MAC will not decrease
* the datarate, in case the LoRaMAC layer did not receive an acknowledgment
*/
uint8_t NbTrials;
}McpsReqConfirmed_t;Only confirmed message use ADR?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.