2022-04-11 3:31 PM
Hi!
Can somebody help, what is the SPI command for triggering sync pulse on PSI5 channel? Auto generated sync pulse mode works fine but i can not find the corresponding SPI command for sync pulse triggering in datasheet.
I would like to use the following:
"Triggering via SPI without upstream data buffer. The microcontroller sends the corresponding SPI command for a sync pulse. The sync pulse trigger generator then internally generates the appropriate sync pulses, based on the specific SPI command sent."
2022-08-31 8:04 AM
Did you try setting the field SYNC1_EN by one?
I am still in the module bring up, but this is the only option might be available?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.