2022-08-18 11:49 AM
The 54AC2525 IBIS Model does not have worst-case corners set up in the model. The model is instead set to run at TYP (3.3V), MIN (2.5V), and MAX (5V). Typically, MIN and MAX are process corners are 3.0V and 3.6V covering the min/max supply. Is there a way to get an ibis model with the actual worst-case/best-case corners at 3.3V? Thanks!
2022-08-18 11:54 AM
This stuff would typically come via your local sales/support office, and business contacts there.
Here, perhaps an Online Support Request directly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.