2016-09-02 8:02 AM
Hello
I am using a Nucleo F103 RB with XNUCLEO-IDW01M1
board to develop the code.I have been successfully using the Update over the air feature for some time.I now have an image file that has grown because of the extra features on the Web pages etcFrom my console I get the following message :-<TX> at+s.httpdfsupdate=192.168.0.12,/outfile.img<RX> Invalid HTTPD_FS image, length (633215)I am not sure if my image file is somehow corrupt or just too large.My previous image files have worked perfectly from a PC set up as web serverand are approx 300k in length.I have tried running Httpd_gen.exe a few times but the same results. Is there a maximum size permitted ?2016-09-02 8:58 AM
Hi Paul,
1Mb flash memory is splitted in 2 different parts: half dedicated to FW-OTA, and half dedicated to FS-OTA. So, 500Kb is maximum allowed size for both commands.CiaojerryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.